{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the part number for the deadfront trim screw used on the NEMA 3R QO and Homeline load centers?
Issue:
Current design repair parts

Product Line:
QO and Homeline load centers

Resolution:
The standard deadfront trim screw is part number 4020513001K, which is a bag of 10 screws. This is the 1/2" long screw used for ALL the QO and Homeline NEMA 3R deadfront trims.

The actual NEMA 3R door/cover mounting screws are different and need to be obtained from the load center repair parts list FAQ for each load center catalog and series number.

The standard NEMA 1 QO and Homeline Cover screws are part number 4020513002K, which is a bag of 10 screws. This is the 3/4" long screw used for ALL the QO and Homeline NEMA 1 covers.

NOTES:
1) Both the above 3/4" and 1/2" screws have the exact same thread and can be use for either the NEMA 1 cover and/or the NEMA 3R deadfront trim if needed.
2) Square D does NOT offer a cover screw longer than the 3/4".
Screw pics

Schneider Electric Canada