{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Generator does not charge my batteries using the XW or SW models?
Generator is not charging the batteries

If the inverter/charger qualifies the signal but the unit goes right away to passthrough, please check the following
Make sure Charger is enabled
Confirm that the Charger Block Start/Stop is not enabled during the times that you want it to charge

NOTE:Ex.  If the Charger Block Start is set at 4:00am and the Charger Block Stop is set at 11:00pm, that means that it will not charge between 4am and 11:00pm.
It would only charge from 11:00pm to 4:00am
Tip:If there is no need to block the charging then set the start/stop times to 12:00am to disable the feature

Schneider Electric Canada

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.