Issue:
Are reduced sound levels offered for the new EX and EXN type of Energy Efficient Transformers?
Product Line:
Low Voltage Transformers.
Environment:
Energy Efficient Transformers.
Cause:
Reduced sound levels needed.
Resolution:
NO Reduced sound levels (e.g. 42DB) – no longer required since the low induction levels required to obtain the new efficiency provide EX transformers that are at least 6dB below NEMA requirements.
Released for:Schneider Electric Canada