{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can two pieces of panelboard cable trough for an NQ/NF column width panel, be spliced together?
Issue:
Can two pieces of panelboard cable trough be spliced together?

Product Line:
NQ/NF Circuit Breaker Panelboards sold and supported in the USA.

Environment:
Installation

Cause:
Product Features

Resolution:
The column-width cable trough needs no splice.  The pieces are made to be connected end to end.

Schneider Electric Canada