{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the torque requirement for the mounting nuts used to secure the lugs provided in the QOL225 and QOL3225 main lug kits to the load center busbars?
Issue:
Specifications

Product Line:
Load Center Accessory

Resolution:
The lug mounting nuts should be torqued to 75 lb-in (8.5 N-m).

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: