Search FAQs
LC1F Mounting Positions
Issue:
What possible mounting positions can the LC1F Contactors be used in without derating?
Product Line:
LC1F contactors - GIC Product
LC1F115 through LC1F2100
Environment:
US Product
Cause:
Product Characteristics
Resolution:
The LC1F contactors can be mounted in a standard vertical orientation with up to a 30 degree incline forward, or they can be rotated 90 degrees counter-clockwise from a standard vertical with no incline forward or backward. These are the only acceptable mounting positions without derating. Please see the attached documentation for additional information.
What possible mounting positions can the LC1F Contactors be used in without derating?
Product Line:
LC1F contactors - GIC Product
LC1F115 through LC1F2100
Environment:
US Product
Cause:
Product Characteristics
Resolution:
The LC1F contactors can be mounted in a standard vertical orientation with up to a 30 degree incline forward, or they can be rotated 90 degrees counter-clockwise from a standard vertical with no incline forward or backward. These are the only acceptable mounting positions without derating. Please see the attached documentation for additional information.
Released for:Schneider Electric Canada
Attachment(s)
Explore more
Range:
Explore more
Range: