{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is there a 3 point latching option for Nema 3R NQ/NF Panelboards?
Issue:
Can a 3 point latching option be used for Nema 3R NQ/NF Panelboards ?

Product Line:
NQ/NF Panelboards

Environment:
Application

Cause:
Product features

Resolution:
Due to Nema 3R's dust tight/watertight rating, this option is not available for NQ and NF Panelboards, only Nema 1 .

Schneider Electric Canada