Issue:
115 degree C temperature rise option for the new EX transformers
Product Line:
LV Transformers
Environment:
EX
Cause:
Product Offering
Resolution:
Yes. EX Transformers that have the letters "HF" in the catalog number are 115C rise Transformers. Example: EX75T3HF, EX150T3HF, etc.
115 degree C temperature rise option for the new EX transformers
Product Line:
LV Transformers
Environment:
EX
Cause:
Product Offering
Resolution:
Yes. EX Transformers that have the letters "HF" in the catalog number are 115C rise Transformers. Example: EX75T3HF, EX150T3HF, etc.