{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Getting error in Powerlink Software LCS --- mscorlib -- Exception has been thrown by the target of an invocation
Issue:
Getting error in Powerlink Lighting Control software LCS --- mscorlib -- Exception has been thrown by the target of an invocation when access Input status.

Product Line:
LCSBASIC, LCSADVANCED

Environment:
XP, Windows 7, Windows 8

Cause:
DPI settings on the computer using LCS is set to something besides "NORMAL" "100%"

Resolution:
In screen resolution change DPI settings to Normal or 100%. Some time it shows up as "text size"

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: