{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the part numbers for the circuit breaker mounting screws used in the NQSFB2Q and NQSFB2HJ subfeed breaker kits?
Issue:
Are the sub feed breaker mounting kit screws available separately for the NQSFB2Q and NQSFB2HJ subfeed breaker kits?

Product Line:
NQ Panelboards

Environment:
NQ panel accessories, subfeed breaker kits

Cause:
replacement parts

Resolution:
The NQSFB2HJ comes with (2) 8-32 x 3.25 inch tapping screws. The part number is HUA14738 for a quantity of 1.

The NQSFB2Q comes with (2) HUA14738 ( 8-32 x 3.25 inch tapping screws) , in addition  NQSFB2Q and NQSFB2HJ subfeed breaker kits to the (2) 8-32 x 2.25 inch tapping screws needed , using part number HUA14740 for a quantity of 1.

Schneider Electric Canada