{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Video: Troubleshooting 2510M Manual Starters installations
Issue:
2510M manual motor starter installation

Product Line:
Type M and T Integral Horsepower Starters

Environment:
US Product

Resolution:
The underlying cause of this issue is almost always incorrect installation or initial reset of the thermal units.
  1. Check if thermal units have actually been bought and installed.  These units require either one or three thermal units depending on whether it is a single phase or three phase unit respectively.
  2. If units have been installed, check to see that the installation has been done properly.  The thermal unit should be installed with the ratchet wheel on the left and with the writing on the brass clearly visible.  The pawl arm extending from the overload block should be on the top side of the wheel  so that the curved piece is able to grab onto the wheel when reset.
  3. If units have been installed correctly, try resetting the device.  The stop button must be pressed very firmly in so that the pawl arms lower against the ratchet wheel and catch.  It is recommended to use both thumbs to press in the stop button so that an appropriate amount of force is used.
Following these directions will solve most issues for new installations.

Please review the following video and attached instruction bulletin for reference to the above steps:

Schneider Electric Canada

Attachment(s)
30072-013-19 2510M, 2510T.pdf [114.05 KB]
Class 2510 Type M Thermal Unit Installation_.pdf [70.02 KB]
Explore more
Range:
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
Product: