{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the watts/volts on the strip heater installed in our Model 6 Motor Control Centers
Issue:
What is the watts and voltage of the standard strip heater installed in our Nema 3R Model 6 motor control centers.

Product Line:
Model 6 MCC's sold and supported in the USA.

Environment:
Installation/Specification

Cause:
Product Characteristics

Resolution:
The standard strip heater is 200 watts, 120V.

Schneider Electric Canada