{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Do the Square D General Duty Safety Switches Contain a Dual Cover Interlock Feature (so can the cover/door be opened, while the switch is ON)?
Issue:
Product Design Features

Product Line:
General Duty Safety switches

Environment:
Operation of switch

Cause:
maintenance

Resolution:
The General Duty Safety Switches DO NOT contain the Dual Cover Interlock feature. Only the Heavy Duty Switches contain the feature.

The Dual Cover Interlock Feature works as follows: If the Safety Switch operating handle is in the 'ON' Position the switch cover(or door) CANNOT be opened. OR if the Switch operating handle is in the 'OFF' position and the cover(or door) is Open, the Switch operating handle CANNOT be moved to the 'ON' position.

Schneider Electric Canada