{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What Replaces the Obsolete SL800 800A Subfeed Lug Kit?
Issue:
What replaces the obsolete SL800 800A subfeed lug kit in an I-Line panelboard?

Product Line:
I-Line panelboards and accessories sold and supported in the USA.

Environment:
Selection

Cause
Replacement

Resolution:
The SL800M5 is the direct replacement for the SL800. It is rated for 3 - 3/0 to 500 MCM conductors.

Schneider Electric Canada

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
Range: