Search FAQs
How to migrate a VIP to a new Power Monitoring Expert system
Issue
When moving an ION Enterprise or Power Monitoring Expert (PME) system to a new machine it may be necessary to maintain all previous data and custom programming associated with the ION Virtual Processor (VIP)
Product Line
ION Enterprise 4.x
ION Enterprise 5.x
ION Enterprise 6.x
Struxureware Power Monitoring 7.0.x
Power Monitoring Expert 7.2.x
Power Monitoring Expert 8.x
Power Monitoring Expert 9.x
Power Monitoring Expert 2020
Power Monitoring Expert 2021
Power Monitoring Expert 2022
Power Monitoring Expert 2023
Environment
All ION Enterprise and Power Monitoring Expert systems.
Cause
Installation of ION Enterprise or Power Monitoring Expert on a new machine creates a newly named VIP. It registers the VIP as the default name for the VIP service without any of the custom programming used in the original system.
Resolution
*Warning: Take backups of any files prior to modifying them. Ensure the backups are in a location that will not be overwritten (i.e. the Desktop).
Move original data into the proper folder structures with the following steps:
- Stop the newly created VIP service
- Open Windows Service manager (Start > services.msc)
- Find the ION Virtual Processor Service
- Right click this service and select Stop
- Collect the vip.cfg and vip.bak files that were backed up on the original machine. These files are located at ...\Power Monitoring Expert\config\cfg\vip in the folder labeled with the desired VIP's name
- On the new machine, place the files collected from step 2 in the same file path as where they were found on the original machine. (Overwrite the existing files with migrated files)
- Collect the vip.cfg file from the original machine located at ...\Power Monitoring Expert\config\diagrams\nd
- On the new machine place the file collected from step 4 in the same file path as on the original machine. (Overwrite the existing file if it exists)
- Return to the Windows Service Manager and start the ION Virtual Processor service which was stopped in step 1.
All previous programming should now be restored to the new machine.
Note 1: If this is a system with multiple VIP source nodes, please refer to FA221411 for instructions on creating new VIP nodes. Afterwards, follow the above steps for moving original data using the newly created VIP folders.
Note 2:
The path for older versions or direct in-place upgrades could be as follows:
- ...\ION Enterprise\Config\cfg\vip
- ...\ION Enterprise\config\diagrams\nd