{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the Product Environment Profile for PM5000 series meters? Are they RoHS Compliant?
Issue:
Customer wants to know if PM5000 series meters are RoHS compliant and needs the Product Environment Profile.

Product Line:
PM5xxx series meters

Environment:
Safety standards

Resolution:
PM55xx series meters are designed in conformity with the requirements of the European RoHS Directive 2011/65/EU.
PM51xx and PM53xx series meters are designed in conformity with the requirements of the European Directive 2002/95/EC of 27 January 2003

For detailed information about the PM5000 series meter Product Environment Profile, see attached files below.

Schneider Electric Canada

Attachment(s)
PM55xx-ENVPEP1310016_V1.pdf [372.85 KB]
PM51xx-PM53xx-ENVPEP1305025_V2.pdf [164.33 KB]