{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Are enclosures only available for I-line II Powerpact busway plug in units?

Issue:
Can the enclosures only be replaced for I-line II Powerpact busway plug in units?

Product Line:
busway

Environment:
I-line II busway

Cause:
Repair parts

Resolution:
No we do not offer enclosures only for the powerpact circuit breaker plug in units for I-line II busway. The entire plug in unit must be replaced. This includes the following busway plug in units starting with:
PHD, PHG, PHJ, PHL, PBLD, PBLG, PBLJ, PBLL, PBLR, PTMG, PTMJ, PTBG , PTBJ , PTRG, PTRJ, and PTRL

Schneider Electric Canada

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: