{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is it possible to convert a QMJ switch to a QMB switch to accept a class R fuse?
Issue:
Can a QMJ switch be changed or modified to accept a class R fuse?

Product Line:
Switches

Environment:
QMB and QMJ

Cause:
Product features conversion

Resolution:
No. The QMJ has a smaller foot print than the QMB switches (regardless of the fuse type). The only fuse the QMJ accepts is the class J. The QMB on the other hand comes with class H fuse clips. You can add a class R rejection kit to it and the load side base assembly can be adjusted to accept class J fuses.

Schneider Electric Canada