{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What is does the 1 suffix represent on Surgelogic MA modules?

Issue:
The difference in UL 1449 Type replacement SPD Modules

Product Line:
Surge Protection Devices

Environment:
IMA

Cause:
Difference

Resolution:
The suffix "1" indicates a Type 1 SPD which is a permanently connected SPD intended for installation between the secondary of the service transformer and the line side or load side of the service equipment overcurrent device. Types 1 and 2 primarily refer to the location within the electrical distribution system where the SPD may be installed.

Without a '1" indicates Type 2 SPD which is a permanently connected SPD intended for installation on the load side of the service equipment overcurrent device connected to a dedicated overcurrent device; including SPDs located at the branch panel.

Schneider Electric Canada

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: