{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Does the EGX150 (Link 150) support Powerlogic and SY/MAX protocols?

Issue
The user needs to know if the EGX150 supports the Powerlogic and SY/MAX protocols.

Product Line
EGX150

Environment
Gateway Protocol Support

Cause
A user needs to convert legacy device protocols such as Powerlogic and SY/MAX from CM2000 series, CM200 series, CM100 series, etc. to Modbus TCP/IP.

Resolution
The EGX150 supports the Powerlogic or SY/MAX protocols. When the 'Transmission Mode' within the serial port setting is automatic, the device allows you to communicate to Modbus RTU, Jbus, and PowerLogic™ (SY/MAX) slave devices on the same daisy chain.

For Master mode, the usage of the COM port is:

  • Modbus RTU devices do not have to be defined in the Device List, but it helps you manage your system.
  • PowerLogic protocol (SY/MAX) devices must be defined in the Device List.


EGX150 supported Protocols (Ethernet):
IPv4/IPv6 - HTTP
FTP
Modbus TCP/IP
SNMP (MIB II)

Schneider Electric Canada