{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the rail splice part number for the NF600SFBJ sub feed breaker kit?
Issue:
Part number for the rail splice for the NF600SFBJ sub feed breaker kit?

Product Line:
NF Panelboard

Environment:
Installation

Cause:
Lost/Ship short

Resolution:
The part number is 80113-561-01 and 2 are required for the NF600SBJ Sub feed breaker kit .
See attached Instruction bulletin.

Schneider Electric Canada

Attachment(s)
NF 400A -600A dual sub feed breaker kit 80043-760-03.pdf [11.77 MB]