{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How many spaces do QOT or HOMT tandem circuit breakers use?
Issue:
Number of spaces tandem breakers use in load centers

Product Line:
Tandem breakers

Cause:
QOT and HOMT Tandem Circuit Breakers

Resolution:
In the load centers that accept tandem breakers, and NOTE, NOT all load centers will accept these tandem breakers, it depends on the load center catalog number. The QOT and standard HOMT tandem breakers only use one pole space in the load center. But the HOMT Quad tandem breakers will use 2 pole spaces in the load center. The QOT and standard HOMT tandem breakers are independent poles of the breaker. The HOMT Quad tandem breaker will consist of one 2pole breaker and two single pole breakers.

Schneider Electric Canada