{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can the 2 pole H and J Frame breakers be used in the J250__ enclosures?

Article available in these languages: Spanish

Issue:
Product design features

Product Line:
Molded Case Circuit Breaker Enclosures

Resolution:
The 2 pole J frame breakers and 2 pole HJL and HLL circuit breakers can be used in the J250__ enclosures. But the 2 pole HDL and HGL breakers CANNOT be used in the J250__ enclosures. The 2 pole HDL and HGL breakers use the H150__ enclosures.

Schneider Electric Canada

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: