{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the phasing for the I-Line breakers or distribution panel used in an single phase Speed D switchboard?
Issue:
What is the phasing for the I-Line breakers or distribution panel used in an SB126IR ? Can a  QBA221502 and a HQO206AC fit ?

Product Line:
Speed D Board

Environment:
SB126IR

Cause:
Installation

Resolution:
​Yes, the bus is phased AC. Approved breakers include QB,Q2-H,QD,QG,QJ,FY,FA,FH,HD,HG,HJ,HL,JD,JG,JJ,JL

Schneider Electric Canada