Search FAQs
Does Square D Schneider have installation instruction bulletins, or maintenance manuals, for Model,4, 5, and 6 Motorcontrol Center that shows the torque values?
Issue:
Is there an installation instruction bulletin or manual available for the Model 4, Model 5 or Model 6 Motor Control Center for the torque values?
Product Line:
Motor control center
Environment:
Model 4, Model 5, Model 6
Cause:
installation, maintenance, torque requirements
Resolution:
The installation and maintenance instruction manual, bulletin, or guide for Model 6 MCC or Motorcontrol Center is located in our technical library. We have attached pages 50 and 51 for the torque values. See the link below for the full instruction bulletin.
https://www.se.com/us/en/search/80459-641-01#
For Model 4 and Model 5 please see the attachments
Released for:Schneider Electric Canada
Attachment(s)
Explore more
Range:
Explore more
Range: