{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is K factor and what does it mean regarding transformers?
Issue:
What does it mean to have a transformer that is K rated?

Product Line:
Transformers

Environment:
Class 7400 low voltage transformers

Cause:
Application, features

Resolution:
K-factor is a weighting of the harmonic load currents according to their effects on transformer heating, as derived from ANSI/IEEE C57.110. The higher the K-factor, the greater the harmonic heating effects.

There are many different loads such as computers, solid state devices and motors which cause a non linear load. These type of loads generate harmonic currents that cause transformers and system neutrals to overheat, which can destroy the transformer.

When a non-linear load is supplied from a transformer,   K-factor transformers withstand the heating effects of harmonic currents created by these type of loads due to their larger winding coil diameters.

Schneider Electric Canada