{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
ENM error: Object reference not set to an instance of an object
Issue
The following error is seen in Monitoring and Diagnostics component of Event Notification Module (ENM):

Error screen in monitoring and diagnostics
HandlingInstanceID: f155d374-d1d5-4c96-8ef8-f8dd3f4d726c
An exception of type 'System.NullReferenceException' occurred and was caught.
-----------------------------------------------------------------------------
02/10/2016 16:05:50
Type : System.NullReferenceException, mscorlib, Version=4.0.0.0, Culture=neutral, PublicKeyToken=b77a5c561934e089
Message : Object reference not set to an instance of an object.

Source : jrr2cetk
Help link :
Data : System.Collections.ListDictionaryInternal
TargetSite : Boolean Evaluate()
HResult : -2147467261
Stack Trace :    at eSolutions.PowerLogic.AlarmGen.Expression.Evaluate() at eSolutions.PowerLogic.AlarmGen.Advanced.Prc_Advanced.AlarmStatus(Object& testValue, String& actCond)


Product Line
Event Notification Module (ENM)

Environment
Monitoring and Diagnostics (http://localhost:85)
Alarm Sentry (http://localhost:83)

Cause
A wrong expression when setting up Advanced Alarm in Alarm Sentry.
The Evaluate() function in ENM code evaluates the syntax and generates an error if it is not correct.  The error message indicates a problem when executing the Evaluate() function.

Resolution
The syntax has to conform to C# and always return a boolean true or false:
if((Double)Source("<tag>")==1)
{return true;}
else
{return false;}
Where the <tag> has to be replaced with an OPC tag.


An example:

if((Double)Source("localhost.ION.OpcDaServer.1.GEN_A.Gen_A_1/Eng Op Mode")==1)
{return true;}
else
{return false;}

Schneider Electric Canada

ENM error: Object reference not set to an instance of an object
Issue
The following error is seen in Monitoring and Diagnostics component of Event Notification Module (ENM):

           Error screen in monitoring and diagnostics
HandlingInstanceID: f155d374-d1d5-4c96-8ef8-f8dd3f4d726c
An exception of type 'System.NullReferenceException' occurred and was caught.
-----------------------------------------------------------------------------
02/10/2016 16:05:50
Type : System.NullReferenceException, mscorlib, Version=4.0.0.0, Culture=neutral, PublicKeyToken=b77a5c561934e089
Message : Object reference not set to an instance of an object.

Source : jrr2cetk
Help link : 
Data : System.Collections.ListDictionaryInternal
TargetSite : Boolean Evaluate()
HResult : -2147467261
Stack Trace :    at eSolutions.PowerLogic.AlarmGen.Expression.Evaluate() at eSolutions.PowerLogic.AlarmGen.Advanced.Prc_Advanced.AlarmStatus(Object& testValue, String& actCond)


Product Line
Event Notification Module (ENM)

Environment
Monitoring and Diagnostics (http://localhost:85)
Alarm Sentry (http://localhost:83)

Cause
A wrong expression when setting up Advanced Alarm in Alarm Sentry.
The Evaluate() function in ENM code evaluates the syntax and generates an error if it is not correct.  The error message indicates a problem when executing the Evaluate() function.

Resolution
The syntax has to conform to C# and always return a boolean true or false:
 
if((Double)Source("<tag>")==1)
  {return true;}
else 
  {return false;}
 
Where the <tag> has to be replaced with an OPC tag.


An example:

if((Double)Source("localhost.ION.OpcDaServer.1.GEN_A.Gen_A_1/Eng Op Mode")==1)
  {return true;}
else 
  {return false;}

Schneider Electric Canada

Explore more
Range:
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
Explore more
Range:
move-arrow-top