Issue
What is the Unit ID in ION Setup for a PM5300 series meter that is connected by Ethernet?
Product Line
PM53xx Meters
Environment
Connecting PM53xx series meter in ION Setup or Modbus Tester.
Cause
Unit ID or Unique Modbus Address is required to read data from ION Setup or Modbus Tester
Resolution
Unit ID is hardcoded to 255 when connecting to the PM53xx by Ethernet directly.
What is the Unit ID in ION Setup for a PM5300 series meter that is connected by Ethernet?
Product Line
PM53xx Meters
Environment
Connecting PM53xx series meter in ION Setup or Modbus Tester.
Cause
Unit ID or Unique Modbus Address is required to read data from ION Setup or Modbus Tester
Resolution
Unit ID is hardcoded to 255 when connecting to the PM53xx by Ethernet directly.