{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What size cords can be used with XACA960 cable sleeve of the XACA pendant stations?

Issue:
Identify the size cords used on the XACA pendant stations

Product Line:
XAC Pendant Stations

Environment:
Push Buttons and Operator Interface

Resolution:
Any sleeved cord from 8mm to 26mm is acceptable, and individual wires should be no thicker than 14 AWG.

Schneider Electric Canada

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: