{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the repair parts for the CHU364, series F5? (may be shown as F05)
Issue:
Repair parts

Product Line:
Canadian Heavy Duty Safety Switch

Resolution:
The repair parts for the CHU364, series F5 (F05) are as follows. No other parts are available.
Complete Line/Load Base - 4056703950 (1 required; includes phynolic base, arc suppressors, lugs, rotor, switching blades)
Line/Load Base mounting screws - 4020546401 (6 required per line base)
Arc Suppressor Assembly - 4056677550 (1 required per phase)
Arc Suppressor mounting screw - 4020514501 (1 required per arc suppressor)
Lug Assembly - 4025136550 (per lug)
Lug Assembly mounting screw - 2140122240
Switch Mechanism - 4056678650
Switch Mechanism mounting screws- 2299940562 (2 required)
Handle Assembly - 4056663550
Lockplate - 4056672101
Lockplate mounting screws - 2299940562 (2 required)
Cover latch and spring - one each of 4056607201 (latch) and 4022304301 (spring)

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: