Issue:
A user would like to add support in PME for a third party Modbus device that does not have a built in device driver.
Product Line:
ION Enterprise 5.6, 6.0, 6.1
StruxureWare Power Monitoring 7.0.x
Power Monitoring Expert (PME) 7.2.x, 8.x
Environment:
Modbus Device Importer
Resolution:
Below is a video demonstrating how to create a custom modbus device driver for any third party device using the Modbus Device Importer.
Note: default measurement labels should be used when naming registers as this will ensure compatability with other PME features.
See KB FA233509: List of 'Official' StruxureWare Power Monitoring Labels
A user would like to add support in PME for a third party Modbus device that does not have a built in device driver.
Product Line:
ION Enterprise 5.6, 6.0, 6.1
StruxureWare Power Monitoring 7.0.x
Power Monitoring Expert (PME) 7.2.x, 8.x
Environment:
Modbus Device Importer
Resolution:
Below is a video demonstrating how to create a custom modbus device driver for any third party device using the Modbus Device Importer.
Note: default measurement labels should be used when naming registers as this will ensure compatability with other PME features.
See KB FA233509: List of 'Official' StruxureWare Power Monitoring Labels
Released for:Schneider Electric Canada
Issue:
A user would like to add support in PME for a third party Modbus device that does not have a built in device driver.
Product Line:
ION Enterprise 5.6, 6.0, 6.1
StruxureWare Power Monitoring 7.0.x
Power Monitoring Expert (PME) 7.2.x, 8.x
Environment:
Modbus Device Importer
Resolution:
Below is a video demonstrating how to create a custom modbus device driver for any third party device using the Modbus Device Importer.
Note: default measurement labels should be used when naming registers as this will ensure compatability with other PME features.
See KB FA233509: List of 'Official' StruxureWare Power Monitoring Labels
A user would like to add support in PME for a third party Modbus device that does not have a built in device driver.
Product Line:
ION Enterprise 5.6, 6.0, 6.1
StruxureWare Power Monitoring 7.0.x
Power Monitoring Expert (PME) 7.2.x, 8.x
Environment:
Modbus Device Importer
Resolution:
Below is a video demonstrating how to create a custom modbus device driver for any third party device using the Modbus Device Importer.
Note: default measurement labels should be used when naming registers as this will ensure compatability with other PME features.
See KB FA233509: List of 'Official' StruxureWare Power Monitoring Labels