{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What's the length of remote display cable that comes with PM5563RD or PM5RD?
Issue
A user may want to know the length of the display cable provided with the PM5563RD meter or PM5RD remote display kit

Product Line
PM5000 series meters

Environment
Metering

Resolution
The PM5563 (complete part number METSEPM5563RD), is provided with a display cable 3 meters long.
The same 3 meters cable is provided  with the PM5000 remote display kit (complete part number for that kit is METSEPM5RD)

The part number for the 3 meter display cable is METSEPM5CAB3.

Other display cable lengths are available:
METSEPM5CAB03 - 0.3m Length Cable Kit
METSEPM5CAB1   - 1m Length Cable Kit
METSEPM5CAB10 - 10m Length Cable Kit

Schneider Electric Canada