{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the maximum number of auxiliary contacts that can be added to 8536/8502 Starter/Contactor
Issue:
Max number of auxiliary contacts to install on a NEMA Type S Contactor/Starter

Product Line:
NEMA Contactors and Starters

Environment:
NEMA Type S Contactors and accessories

Cause:
Product Specifications

Resolution:
The maximum number of aux contacts listed are in addition to the supplied internal holding contact

Size 00 Max three poles - 4 single circuit auxiliary contacts (NO or NC) if second internal auxiliary contact is not used
Size 0-2 Max three poles - 4 single circuit auxiliary contacts (NO or NC)*
Size 0-2 Max three poles - 2 single circuit auxiliary contacts (NO or NC) plus one power pole adder
Size 0-2 four or five poles - 2 single circuit auxiliary contacts (NO or NC)
Size 3-4 two to five poles - 3 single circuit auxiliary contacts (NO or NC)
Size 5 two or three poles - 2 single circuit auxiliary contacts (NO or NC) plus one power pole adder
Size 6-7 two or three poles - 3 single circuit auxiliary contacts (NO or NC)
Size 6-7 two or three poles - 2 single circuit auxiliary contacts (NO or NC) plus one power pole adder

*when adding 4 external auxiliary contacts to one size 0 or 1 contactor, remove one of the return springs

See part number table below for selection:
For Use WithKit descriptionOrdering Information
TypeNEMA SizeClass 9999
Type
External - Field Convertible
SA-SJ00-71 N.O. contactSX6
1 N.C. contactSX7
1 N.O. and 1 N.C. isolated contactsSX8
1 N.O. overlapping contactSX9 *
1 N.C. overlapping contact SX10 *
External - Non-Convertible
SA-SJ00-71 N.O. ContactSX13
1 N.C. ContactSX14
1 N.O. and 1 N.C. isolated contactsSX15
1 N.O. overlapping contactSX16 *
1 N.C. overlapping contact SX17 *
Internal - Non-Convertible
SA-SD00-21 N.O. ContactSX11 #
1 N.C. ContactSX12 #

* - Types SX9 and SX10 or types SX16 and SX17 must be used together and mounted on the same side of the contactor. They are suitable for applications where it is necessary for a normally open contact to overlap a normally closed contact.
# - Types SX11 and SX12 are not for use on NEMA size 3 or larger. Internal contacts can also be used on Class 2510 types M and T manual starters

Schneider Electric Canada

Explore more
Product:
Range:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product:
Range: