{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What is the weather shield for EX225T3HCU? 25J enclosure.

Issue:
The EX225T3HCU is in a 25J enclosure and Digest 177, page 14-6 states it is factory assembled only.

Product Line:
Transformers

Environment:
weather shield, 25J, EX transformer, accessories

Cause:
Looking for a weather shield to add to a transformer that has already shipped

Resolution:
7400WS25J is the field installable weather shield for the 25J transformer enclosures.

Schneider Electric Canada