{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
​What happens when you remove a rating plug from a Micrologic trip unit?
Issue:
Removal of rating plug from a Micrologic Trip Unit

Product Line:
Molded Case Circuit Breakers / Air Circuit Breakers

Resolution:
Removing the rating plug from the Micrologic trip unit automatically reduces the rating of the breaker to value of 40% (e.g. a 1000 A breaker becomes a 400 A breaker).
This applies to the following breakers and trip units:

Circuit Breakers
PowerPacT P and R
MasterPact NT and NW

Micrologic Trip Units
Standard 2.0, 3.0, 5.0
Ammeter 2.0A, 3.0A, 5.0A, 6.0A
Power 5.0P, 6.0P
Harmonic 5.0H, 6.0H

Schneider Electric Canada