{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can Smart Cell be used in QED2 Switchboard construction?
Issue:
Use Smart Cell in QED2 Switchboard construction

Product Line:
Smart Systems

Environment:
Products sold and used in the United States

Resolution:
Yes, Smart Cell CAN be used in QED2 construction as an after shipment product, however Schneider Electric assembly plants will not utilize Smart Cell in QED2 Construction, since the new QED2 Series 2 I-Line interior sections include a small instrument compartment running across the top, which is designed to provide similar functionality for mounting “Smart” components without taking up I-Line mounting space.

Schneider Electric Canada