{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Video: How to replace the contacts in a NEMA size 00, 0, and 1 starter
Issue:
Are there instructions on how to change the contacts on a Nema starter?

Product Line:
NEMA size 00, 0, and 1, NEMA Type S starters, 8536SAO, 8536SBO, 8536SCO

Environment:
Products sold in the US

Resolution:

With line and control power completely removed from the starter, you will need to follow the below steps:

  1. Remove wiring from both coil terminals
  2. Loosen the power plant screws holding the main contactor body together
  3. Remove power plant consisting of coil, armature, magnet, and contact carrier with removable contacts.
  4. Remove the movable contacts by depressing them down and rotating the contact and sliding through opening on the carrier. At this step also remove the spring and spring guide.
  5. Replace contact, spring and guide spring first, guide and contact.
  6. Repeat Steps 4-5 for each movable contact
  7. Remove the 6 stationary contacts by removing the screw holding them to the base.
  8. Re-install the power plant and re-install any wiring making sure to follow your supplied wiring diagram.
Note: Tighten all screws to recommended torque settings shown in attached instruction bulletin.

Schneider Electric Canada

Attachment(s)
30072-013-23.pdf [208.37 KB]
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.