{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Optional Device Driver for Energy Meter in Power Monitoring Expert 7.2.x and 8.x
Issue
There is no default support for this device type in Power Monitoring Expert.

Product Line
Energy Meter (EME and EMB)
Power Monitoring Expert (PME) 7.2.x
Power Monitoring Expert (PME) 8.x

Environment
Limited Edition (LE) driver which supports real time registers and PC based logging

Cause
To be able to add one or more of these devices to Power Monitoring Expert system.

Resolution

The attached ZIP file includes the:
- installer (.msi file) to add the new device type
- register list in Excel

Once the installer is run, the device type can be seen in Management Console:



And Vista diagrams are added to Config folder:

Schneider Electric Canada

Attachment(s)
PME_7_EnergyMeterDeviceDriver.zip [635.24 KB]
PME_8_Energy_Meter_DT.zip [307.65 KB]
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.