{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

How do you install or mount the PTB316GH or PTB516GH Horizontal Plug in Tap boxes? Where are the mounting instructions?

Issue:
Are mounting instructions available for the PTB316GH or PTB516GH Horizontal Plug in Tap boxes?

Product Line:
Busway

Environment:
PTB316GH and PTB516GH

Cause:
Installation and mounting

Resolution:
The PTB (800 - 1600A)  horizontal plug in cable tap boxes are installed in a plug in opening in the Plug in style 800A - 1600A busway. (***Cannot be used in 800A copper Plug in busway). The mounting instructions are located on the inside cover of the tap box. We have also included a copy of those instructions below for review.

Schneider Electric Canada

Attachment(s)

PTB tap box 4512387101(PTB1600 Horizontal).pdfPTB tap box 4512387101(PTB1600 Horizontal).pdf [127.09 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: