Search FAQs
How long is the 33195 handle extension for PowerPacT M and P breakers?
Issue:
How many inches does the 33195 add to the handle length?
Product Line:
Molded Case Circuit Breakers
Resolution:
The 33195 handle extension for PowerPacT M and P frame breakers fits over and covers up the standard breaker handle.
When installed, it is approximately 5.5" in length.
![Pic of breaker handle Pic of breaker handle](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0151H000008zqfhQAA&oid=00DA0000000abSm)
How many inches does the 33195 add to the handle length?
Product Line:
Molded Case Circuit Breakers
Resolution:
The 33195 handle extension for PowerPacT M and P frame breakers fits over and covers up the standard breaker handle.
When installed, it is approximately 5.5" in length.
Released for:Schneider Electric Canada
Explore more
Range:
Explore more
Range: