Search FAQs
Does Square D offer replacement enclosures or doors for the 8940SSE4050 Well-Guard Control Pump Panel?
Issue:
Replacement enclosures or doors for the 8940SSE4050 Well-Guard Control Pump Panel
Product Line:
Well-Guard Control Pump Panel, Full Voltage, Type NS, SS, XS
Environment:
3 pole Polyphase, 480V, 50-60 Hz Fusible Pump Panel
Cause:
Hit the front of their Pump Panel with a forklift , need replacement front or complete enclosure.
Resolution:
No, Square D do not sell the doors or enclosures ONLY for the 8940SSE4050 pump panels.
Replacement enclosures or doors for the 8940SSE4050 Well-Guard Control Pump Panel
Product Line:
Well-Guard Control Pump Panel, Full Voltage, Type NS, SS, XS
Environment:
3 pole Polyphase, 480V, 50-60 Hz Fusible Pump Panel
Cause:
Hit the front of their Pump Panel with a forklift , need replacement front or complete enclosure.
Resolution:
No, Square D do not sell the doors or enclosures ONLY for the 8940SSE4050 pump panels.
Released for:Schneider Electric Canada
Explore more
Range:
Explore more
Range: