Issue:
MCC Conversion Accessory
Product Line:
Circuit Breakers
Environment:
Powerpact H, J, L
Resolution:
The MCC Conversion Accessory (S429341 for H and J; S32606 for L) is added to the direct-mount rotary handle to add the following functions to the handle:
Machine-tool control in compliance with CNOMO Control of a machine-tool is achieved by adding kit S32602 to the standard handle for L frame (S29342 for H, J frames is obsolete).
In addition to the standard functions, the kit offers the characteristics listed below:
MCC Conversion Accessory
Product Line:
Circuit Breakers
Environment:
Powerpact H, J, L
Resolution:
The MCC Conversion Accessory (S429341 for H and J; S32606 for L) is added to the direct-mount rotary handle to add the following functions to the handle:
- IP Degree of protection IP43, IK07. The IP is increased by a built-in gasket.
- Door locking depending on device position.
- The door cannot be opened if the circuit breaker is ON or in the tripped position. For exceptional situations, door locking can be temporarily disabled with a tool to open the door when the circuit breaker is closed. This operation is not possible if the handle is locked by a padlock.
- Circuit-breaker closing is disabled if the door is open. This function can be deactivated.
Machine-tool control in compliance with CNOMO Control of a machine-tool is achieved by adding kit S32602 to the standard handle for L frame (S29342 for H, J frames is obsolete).
In addition to the standard functions, the kit offers the characteristics listed below:
- Enhanced waterproofing and mechanical protection to IP54, IK08.
- Compliance with CNOMO E03.81.501N.