Product Line:
Switching and Controlling, Partner products, Schneider Electric offer, NEMA Starter, IEC Starter
Resolution:
The Schneider Electric Motor Starter Solution Guide allows you to create and save projects for later reference. When creating a new project you will see a catalog section and a solution section. To make a selection follow these steps:
Please see below video for quick reference.
Switching and Controlling, Partner products, Schneider Electric offer, NEMA Starter, IEC Starter
Resolution:
The Schneider Electric Motor Starter Solution Guide allows you to create and save projects for later reference. When creating a new project you will see a catalog section and a solution section. To make a selection follow these steps:
- Select Voltage (we offer selections from 120VAC single phase up to 600VAC three phase)
- You can filter your selection based on the following fields (Each filter will have a help file attached for explanation assistance found using the paper icon on each filter)
- SCCR
- Motor Rated Current
- Motor Rated HP
- Combination Starter Constuction Type
- Configuration
- Overload Type
- Overload Trip Class
- Overload phase Sensitivity
- Choose solution based on remaining selections
Please see below video for quick reference.
Released for:Schneider Electric Canada