{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the BTU for the EX225T3H at no load to full load?
Issue:
What is the heat loss in BTU for the EX225T3H at no load to full load?

Product Line:
General Purpose Dry Type 600 Volts and Below,  EX

Environment:
EX225T3H

Resolution:
Per the Low Voltage Distribution Transformers Catalog 7400CT1501, page 11 provided the core loss from No Load to Full Load
No Load: 328 watts
1/6 load = 445 watts /1517 BTUs/Hr
1/4 load = 590 watts / 2014 BTUs/Hr:
1/2 load = 1378 watts / 4700 BTUs/Hr:
3/4 load = 2689 watts / 9176 BTUs/Hr:
Full watts = 4526 watts / 15443  BTUs/Hr.

Schneider Electric Canada

Attachment(s)
7400CT1501.pdf [3.8 MB]
Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: