{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Can you install 3 pole branch (feeder) breakers in a 3 phase MPZ and MPZB Mini Power Zone?

Issue:
Can you install 3 pole branch (feeder) breakers in a 3 phase MPZ and MPZB Mini Power Zone?

Product Line:
Mini Power Zone

Environment:
MPZ and MPZB Mini Power Zone

Cause:
Product features

Resolution:
Yes they can use 3 pole breakers in both the MPZ and MPZB Mini Power Zones. There is some published misinformation that just states 1 or 2 poles
but all three phase MPZ and MPZB  accept 3 pole breakers.

Schneider Electric Canada