{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Hold down clip - RPZF2 and RPZF4

Issue:
Is a hold down clip available for the RPZF2 and RPZF4 sockets?

Product Line:
Relays and Timers

Environment:
Zelio Relays

Cause:
Product Specifications

Resolution:
These relay sockets do not require hold down clips as the relay is seated securely without it.

Schneider Electric Canada

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: