{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the impedance for the 5S1F transformer?
Issue:
%IZ)for the 5S1F transformer

Product Line:
General Purpose Dry Type 600 Volts and Below

Environment:
Resin Encapsulated, Singe Phase Transformer, 5kVA, 240 x 480 Vac Primary, 120/240 Vac Secondary. 60 Hz; UL/cULus Listed

Resolution:
The Impedance for the 5S1F  Resin Encapsulated, Singe Phase Transformer is 3.58% .

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: