{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Video : How to use ION OPC Test Client to read OPC tags in PME?

Issue
How to use ION OPC Test Client (the built-in OPC Test Client utility in PME) to read OPC tags off of the devices that are connected to the PME.

Product Line
ION Enterprise 5.6, 6.0, 6.1
StruxureWare Power Monitoring 7.0.x
Power Monitoring Expert (PME) 7.2
Power Monitoring Expert (PME) 8.x
Power Monitoring Expert (PME) 9.x
Power Monitoring Expert (PME) 2021
Power Monitoring Expert (PME) 2022
Power Monitoring Expert (PME) 2023

Environment
OPC Test Client utility

Resolution
Below is a video showing how to use the OPC Test Client to read OPC tags off of the devices connected with the PME.

Schneider Electric Canada

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: