undefined undefined
{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
Why does the QOGP3P6036 generator panel utilize a 3 pole breaker to switch from utility to generator?
Issue:
Product Design Features

Product Line:
Canadian QO Generator Panels

Resolution: 
 
The Canadian Electrical Code requires the neutral conductor to be switched with the line conductors for a utility/generator application. Therefore, the 3 pole breakers are used to allow both line conductors and the neutral conductor to be switched (or turned ON and OFF) when switching between utility and generator power.

Schneider Electric Canada

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: