{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Does Schneider Electric SPD's have joule ratings?
Issue:
Joule rating for SPD.

Product Line:
Surge Protective Device

Environment:
EMA SPD, EBA SPD, HWA, TVSS, Surgelogic

Resolution:
Joule ratings are not a recognized indication of protection and not an accurate rating of performance. In the surge protection industry the proper means of determining the protection level is the kA rating, Peak Current Rating (Maximum Current Rating) is the most current that the MOV device can handle without suffering irreversible damage.

Schneider Electric Canada

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: